See-through TV screens may have been all the rage at this year’s CES in Las Vegas, and we have to admit, we’re fans. But, for us, the excitement lies in all the possible ways this technology can be used in our world of displays.
As you’re no doubt aware, a see-through or transparent electronic display allows the user to see what is shown on the screen while still being able to see through it. It’s an emerging market that has many potential uses and cell phones or tablets are the immediate choices that spring to mind. In augmented reality, for example, a tablet with a see-through display could the street onto the screen – like a real-time Google Street View.
A device using a transparent display will have much higher resolution and will therefore the display will be far more realistic than video augmented reality, which takes video, adds its own supplement to it, and then displays that onto the screen. Surely, it’s simpler to display the addition onto the see-through screen instead?

Other important applications for this type of display are in head-up displays, digital signage, and general large-scale spatial light modulation.
The 10.1” monitor with a transparent TFT in this picture, for example, offers many excellent benefits. It’s equipped with a Multitouch PCAP which will recognise up to 10 fingers, has a GG (Glass-Glass) structure, which makes the stack thin and light, and 1.8mm coverglass for reliability and a long life.
Clarity and brightness
The built-in TFT panels have a brightness of 200 cd/m², a contrast ratio of 800:1 and a resolution of 1280 x 800 pixels for clear image display. The viewing angles of 85° from all directions are generous and ensure optimal visibility.
And ease of control
Essentially, it’s a transparent Android Tablet. Albeit one with a powerful Rockchip Cortex A55 Quad Core, 2G DDR3 RAM, Micro SD up to 128Gb and WIFI. It can, of course, play fancy videos, pictures and sounds, but you can place real objects behind the transparent TFT, then make them visible or hidden just by simply pressing on the touchscreen.
Our experts are on hand to guide you in the creation of display or touch solutions that meet your requirements. Find out how Avnet Embedded can propel your product innovation and get in touch today.
Talk to the experts!
Let us know about your product or your challenge and our team will get in touch to discuss how we can help.