PCAP in automotive applications? Yes, we can!
Capacitive sensors are great – highly reliable and have a wide range of functions. You can’t argue with their usefulness in household electronics, especially as panels in such products are becoming thinner and lighter with almost every iteration. In the automotive world, however, this isn’t exactly desirable. In this industry, sensitive sensor technology is subject to stricter requirements, both in terms of service life and environmental influences.
AUO Display+: high, customizable performance without the price tag
Thin, light, cost effective, but with industrial grade reliability and performance, AUO Display+ 15.6” integrated touch solutions are perfect for a range of indoor uses – in-flight entertainment, home automation panels, Point of Sale and kiosk applications.
By popular demand – the MipiPlus 7”. New size, same great performance
We knew the launch of MipiPlus in February would be popular, but we’ve had such a great response to the 7.84” size that we’re now adding the 7” (17.78 cm) screen size to our portfolio. Integrating MIPI display products can be a complex process, but our significant experience in the field has given plenty of customers confidence to partner with Avnet Embedded for the journey.
Small, fast and functional – meet the MipiPlus 4”
When we speak to our customers about MIPI Display products, they all agree that it’s a great interface that comes with some implementation challenges. However, working with Avnet Embedded means that they have a partner with plenty of experience in integrating MIPI into a range of industrial and medical products and our portfolio just keeps growing.
Avnet Embedded expands its broad SMARC™ module product portfolio to open up new markets and applications
The compact SMARC™ computer-on-module standard has experienced tremendous success, especially for low-power applications in different markets. Avnet Embedded, one of the leading manufacturers of embedded modules, has a broad SMARC™ product portfolio with scalable processor technologies and interface features and offers its customers comprehensive design support.
Spotlight on Embedded – March 2023
Welcome to the March issue of Avnet Embedded Spotlight. This month we’ve given a quick round up of the brilliant Embedded World show which happened in Nuremberg on the 14th – 16th March. We’re also giving you details on the latest SBCs, motherboards and more!