Posts

Bringing clarity to the world of MIPI and LVDS
Where displays are concerned, plenty of acronyms fly around. MIPI is one, LVDS and RGB/TTL are some others. You’d expect all three to be completely different, but life is never that precise, is it? For example, MIPI displays also use LVDS standards and as puzzling as that might sound, there are actually some fairly sound reasons for it.
Landscape or portrait, MipiPlus 5.5” fills the gap
Thin, light, low power, low brightness, our industrial customers have fully embraced the MipiPlus range for its excellent value and our ability to integrate it into their products seamlessly. So, it will come as no surprise that we are able to offer another new addition to our ever-growing portfolio.

By popular demand – the MipiPlus 7”. New size, same great performance
We knew the launch of MipiPlus in February would be popular, but we’ve had such a great response to the 7.84” size that we’re now adding the 7” (17.78 cm) screen size to our portfolio. Integrating MIPI display products can be a complex process, but our significant experience in the field has given plenty of customers confidence to partner with Avnet Embedded for the journey.
MipiPlus – the everyday touch display with industrial speed
Display products with MIPI (Mobile Industry Processor Interface) had previously been limited to purely high-volume consumer products, most notably smart phones. Recently, however, there has been a steady increase of MIPI products across industrial and medical applications and this has created more room for them mainly in handheld applications and sizes due to lower power requirements.