Avnet Embedded is becoming Tria! Visit our new website here.

Avnet Brings High Performance on ARM-based processors to Two New Computer-on-Modules in Collaboration with Qualcomm

Octal core 6nm processor with highest ARM* performance on SMARC* and best in class power to performance ratio

Nuremberg, Germany – April 10, 2024 – In collaboration with Qualcomm Technologies, Inc., Avnet (Nasdaq: AVT) is launching two new ARM*-based System on Modules (SoM) at Embedded World 2024. These modules, powered by Qualcomm® QCS5430 and Qualcomm® QCS6490 processors, bring a new level of performance to Avnet’s portfolio of SMARC modules.

SMARC* (Smart Mobilty ARCHitecture) is a versatile small form factor computer module for applications that require low power, low costs and high performance.

“Our new collaboration with Qualcomm Technologies allows Avnet to extend our offerings of modules to include high-end ARM technology,” said Thomas Staudinger, president, Avnet Embedded. “These solutions deliver powerful performance and are purpose-built for industrial and commercial IoT applications. These applications include ruggedized handhelds and tablets kiosks, industrial scanners, dash cameras, point-of-sales systems and human machine interface systems.”

“The convergence of edge computing and AI is transforming industries, ushering in a new era of intelligent devices,” said Enrico Salvatori, Senior Vice President and President, Qualcomm Europe/MEA of Qualcomm Europe, Inc. “Qualcomm Technologies is proud to announce our industrial IoT collaboration with Avnet and support the launch of their new AI-capable SMARC modules, powered by the QCS6490 and QCS5430 processors.”

SM2S-QCS6490 offers maximum CPU, GPU and NPU performance at a well-balanced power consumption, whereas the SM2S-QCS5430 offers a good balance between compute, power consumption and price.

Product features:

 

  • MSC SM2S-QCS6490 SMARC 2.1.1 module family
    • Powered by the 6nm Qualcomm® QCS6490 processor
      • Integrates Qualcomm® Kryo™ 670 CPU which contains up to eight cores (four ARM Cortex*-A78 Cores, four ARM Cortex-A55 cores)
      • Qualcomm® Adreno™ 643 GPU
      • Qualcomm® Adreno™ 633 VPU
      • Latest re-engineered Qualcomm® Hexagon* processor
    • The GPU supports video encode/decode at up to 4K30/4K60 and many different display options (LVDS, MIPI-DSI, eDP/DP).
    • It delivers powerful edge AI for high-performance with up to 12 TOPS at low power and massive camera support with 4 MIPI-CSI inputs

 

  • MSC SM2S-QCS5430 SMARC 2.1.1 module family
    • Powered by the 6nm Qualcomm® QCS5430 processor
      • Integrates Qualcomm® Kryo™ 670 CPU which contains up to six cores (two ARM Cortex-A78 cores, four ARM Cortex-A55 cores)
      • Qualcomm® Adreno™ 642L GPU (graphic processing unit)
      • Qualcomm® Adreno™ 633 VPU (vision processing unit)
      • Latest re-engineered Qualcomm® Hexagon™ processor
    • The GPU supports video encode/decode up to 4k30/4k30 and many different display options (LVDS, MIPI-DSI, eDP/DP).
    • It delivers powerful edge AI for high-performance with up to 3.5 TOPS at low power and massive camera support with 4 MIPI-CSI inputs

Visit the Avnet Embedded booth 1-510 at embedded world to see these boards.

For more information visit:

https://embedded.avnet.com/product/msc-sm2s-qcs6490/

https://embedded.avnet.com/product/msc-sm2s-qcs5430/

Qualcomm, Kryo, Adreno and Hexagon are trademarks or registered trademarks of Qualcomm incorporated. Qualcomm branded products are products of Qualcomm Technologies, Inc. and/or its subsidiaries. Qualcomm patented technologies are licensed by Qualcomm Incorporated.

*Trademarks and brands are the property of their respective owners.

MSC SM2S-QCS6490

MSC SM2S-QCS5430

Copyright ©2024 Avnet, Inc. All rights reserved.