Entries by

Avnet Embedded launches compact SMARC module family based on Intel® Atom® x7000E Series processors with up to eight cores

Stutensee, Germany – February, 2023 – Avnet Embedded is expanding its comprehensive SMARC™ product portfolio including announcing availability of the scalable MSC SM2S-ALN module family. These boards integrate an Intel® Atom® processors x7000E Series, Intel® Core™ i3 processor or Intel® Processors N Series (former codenamed “Alder Lake N”). Depending on processor type, the thermal design power (TDP) is between 6W and 15W providing less power dissipation. Two, four or eight cores are available to scale the CPU and graphics performance.

Avnet Embedded brings full Windows 10 IoT on industrial Arm-based SMARC module platform with NXP i.MX 8M Plus SoCs

Stutensee, Germany – March, 2023 – Avnet Embedded has developed an industrial Arm®-based embedded platform with an SMARC™ embedded compute module running the full Microsoft Windows® 10 IoT Enterprise LTSC (Long-Term Servicing Channel) operating system without modification. The advantage is that customers can easily install Windows 10 IoT Enterprise on Avnet Embedded’s MSC SM2S-IMX8PLUS modules integrating an i.MX 8M Plus applications processor from NXP™ Semiconductors and are able to use standard API32 PC applications without re-compilation or re-writing. At embedded world 2023, a demo platform is shown on Avnet Embedded’s Booth 510 in Hall 1 and on Avnet Silica’s Booth 111 in Hall 3A.

RASynBoard brings low-power, edge AI processing to embedded sensor applications.

PHOENIX – March 7, 2023 – The RASynBoard development kit from Avnet (Nasdaq: AVT) can help hardware and software design engineers and embedded AI developers quickly adopt edge AI capabilities into their products, making them more efficient, accurate and reliable. It was created in collaboration with Renesas, Syntiant, TDK, and Edge Impulse, and will be demonstrated in the Avnet Embedded booth (1-510) at the Embedded World Exhibition and Conference, March 14-16, in Nuremberg, Germany.

How we’re engineering touch screens to eliminate ghost touch in mission-critical applications

We build many applications for customers that require absolute precision and reliability for environments where safety and accuracy are important.

We have been working with customers recently on engineering touch screens to absolutely eliminate any chance of ghost touch (false signals of touch inputs on a screen). This has required some creative thinking and deep-level engineering from our in-house display experts.

MipiPlus – the everyday touch display with industrial speed

Display products with MIPI (Mobile Industry Processor Interface) had previously been limited to purely high-volume consumer products, most notably smart phones. Recently, however, there has been a steady increase of MIPI products across industrial and medical applications and this has created more room for them mainly in handheld applications and sizes due to lower power requirements.

Spotlight on Embedded – February 2023

Welcome to our second issue of Avnet Embedded Spotlight – an Embedded World Special. This month we’re focusing on the upcoming Embedded World show in Nuremberg from the 14-16th March. Visit us on booth Hall 1-510 to speak with our experts about Compute, Displays and Software solutions and find out how we can help you to get your product to market faster, better and stronger

One code wonder: why SimpleSwitch will change your software development process forever

It’s a truth universally accepted that the work of software developers is inextricably linked to the hardware their code will finally run on. So, when the hardware changes, so must the code. It’s what has always happened but doesn’t make the process any less frustrating when it comes to meeting tight go-to-market deadlines, or when suddenly your chosen compute modules are unavailable. In these difficult circumstances, developers have always had to suck it up and start from scratch or simply…wait.