Landscape or portrait, MipiPlus 5.5” fills the gap
Thin, light, low power, low brightness, our industrial customers have fully embraced the MipiPlus range for its excellent value and our ability to integrate it into their products seamlessly. So, it will come as no surprise that we are able to offer another new addition to our ever-growing portfolio.

Spotlight on Embedded – May 2023
Welcome to the May issue of Avnet Embedded Spotlight. This month we’ve got new products around AIoT from our franchise partners, motherboards and a reminder all about displays. Let us know if there is anything you’d like to see in an up and coming issue of Spotlight. And don’t forget, if you have an embedded project you’d like to talk about with our team, we’re here to help!

Intel Core processors on COM Express and COM-HPC computing platforms: high performance for AI applications
To support the development of demanding industrial products, Avnet Embedded offers a broad portfolio of innovative embedded computing modules based on powerful 13th and 12th Gen Intel Core series processors.
Another new arrival! 10.1” joins the MipiPlus family
It only feels like a few minutes ago that we shared the news of our MipiPlus 7”, 7.8” and 4” products, but already we have another addition to offer. It’s a testament not only to the popularity of MipiPlus, but the speed at which we are able to launch new tested and proven variations into our portfolio – especially one with an interface as challenging to integrate as MIPI.

Spotlight on Embedded – April 2023
Welcome to the Spring edition of Avnet Spotlight. We’ve got lots of exciting new products to update you on this month across compute, displays and from our partners, too. If you would like to know more, or have a specific embedded project you’d like to discuss, you can always contact our team – we’d love to hear from you.

By popular demand – the MipiPlus 7”. New size, same great performance
We knew the launch of MipiPlus in February would be popular, but we’ve had such a great response to the 7.84” size that we’re now adding the 7” (17.78 cm) screen size to our portfolio. Integrating MIPI display products can be a complex process, but our significant experience in the field has given plenty of customers confidence to partner with Avnet Embedded for the journey.

Small, fast and functional – meet the MipiPlus 4”
When we speak to our customers about MIPI Display products, they all agree that it’s a great interface that comes with some implementation challenges. However, working with Avnet Embedded means that they have a partner with plenty of experience in integrating MIPI into a range of industrial and medical products and our portfolio just keeps growing.

Spotlight on Embedded – March 2023
Welcome to the March issue of Avnet Embedded Spotlight. This month we’ve given a quick round up of the brilliant Embedded World show which happened in Nuremberg on the 14th – 16th March. We’re also giving you details on the latest SBCs, motherboards and more!

Avnet Embedded announces complete starter kit for new SMARC modules based on NXP’s i.MX 93 applications processors
Stutensee, Germany – February, 2023 – Avnet Embedded is launching a comprehensive starter kit for its scalable MSC SM2S-IMX93 SMARC 2.1.1™ module family based on NXP™ Semiconductors’ i.MX 93 applications processors. The MSC SM2-SK-IMX9-EP1 SMARC 2.1.1 starter kit contains all necessary components to quickly enable the customer to evaluate the MSC SM2S-IMX93 modules and start application development.

Avnet Embedded launches compact SMARC module family based on Intel® Atom® x7000E Series processors with up to eight cores
Stutensee, Germany – February, 2023 – Avnet Embedded is expanding its comprehensive SMARC™ product portfolio including announcing availability of the scalable MSC SM2S-ALN module family. These boards integrate an Intel® Atom® processors x7000E Series, Intel® Core™ i3 processor or Intel® Processors N Series (former codenamed “Alder Lake N”). Depending on processor type, the thermal design power (TDP) is between 6W and 15W providing less power dissipation. Two, four or eight cores are available to scale the CPU and graphics performance.