Another new arrival! 10.1” joins the MipiPlus family
It only feels like a few minutes ago that we shared the news of our MipiPlus 7”, 7.8” and 4” products, but already we have another addition to offer. It’s a testament not only to the popularity of MipiPlus, but the speed at which we are able to launch new tested and proven variations into our portfolio – especially one with an interface as challenging to integrate as MIPI.
Innolux High Brightness TFT displays: designed for the great outdoors
Plenty of displays need to be able to cope with the varying demands of outdoor use – think EV chargers, construction sites, agricultural vehicles, boats and many more. Displays in these highly variable locations are not only exposed to the elements but feel the full force of heavy duty use every day. As a result, Innolux has launched a new line of high brightness TFT displays that are more than up to the challenge.
Upgrade your input and swap membrane keys for PCAP
We are frequently asked if we can replace old membrane keypads with a new PCAP design. It makes sense, as the membrane design can present many problems – particularly as it ages. Simply put, membrane keys are less durable and their PET foil, which controls responsiveness, can and will break with frequent use.
Intel Core processors on COM Express and COM-HPC computing platforms: high performance for AI applications
To support the development of demanding industrial products, Avnet Embedded offers a broad portfolio of innovative embedded computing modules based on powerful 13th and 12th Gen Intel Core series processors.
Spotlight on Embedded – April 2023
Welcome to the Spring edition of Avnet Spotlight. We’ve got lots of exciting new products to update you on this month across compute, displays and from our partners, too. If you would like to know more, or have a specific embedded project you’d like to discuss, you can always contact our team – we’d love to hear from you.