Streamlining Development: SimpleSwitch™ and The Embedded Kit

This episode dives into two powerful tools for embedded development: SimpleSwitch™ and The Embedded Kit. We'll explore what each offers, how they work, and how they can work together to streamline your embedded development process.

Widen your view – with the MipiPlus 6.8”

The keen-eyed among you will have noticed that every couple of months we share news of an addition to our MipiPlus range. Well, it’s a product family that just keeps growing. Why? Because you want it to. And today we’re welcoming the MipiPlus 6.8”.
Software Sessions

Develop and Debug Qt Applications on SMARC Modules with SimpleSwitch™

In this blog post, we'll guide you through developing and debugging Qt applications directly on SMARC modules using SimpleSwitch™.

Transparent screens made clear

See-through TV screens may have been all the rage at this year’s CES in Las Vegas, and we have to admit, we’re fans. But, for us, the excitement lies in all the possible ways this technology can be used in our world of displays.
Software_Sessions

Develop and Debug Flutter Apps Directly on SMARC Modules with SimpleSwitch

In this episode, I'll show you how to develop and debug Flutter applications directly on Avnet Embedded SMARC modules using SimpleSwitch™. Buckle up for advanced features like Hot Reload and DevTools at your fingertips!

Develop Directly your web application with Node.js and SimpleSwitch™ on a Compute Module

Why Node.js on a Compute Module? Developing your application backend in JavaScript using Node.js offers several advantages. It's a familiar language for many developers, allows for rapid prototyping, and boasts a rich ecosystem of libraries and frameworks. Using a Compute Module provides a powerful and flexible platform for deploying your application directly on the device.
Embedded Software Sessions Thumbnail

Harnessing the Power of Chromium for Embedded Web Applications

Following up on our episode about deploying static websites, we'll explore how to leverage Chromium on embedded systems with SimpleSwitch™.
Embedded Software Sessions thumbnail

Effortless Web Application development on Avnet Embedded SMARC Modules Using SimpleSwitch and VS Code

In this epsiode, we'll delve into the process of deploying and debugging web applications directly on i.MX8M Plus SMARC modules using SimpleSwitch and VS Code. This streamlined approach facilitates the seamless testing and refinement of HMIs on embedded devices.

Bright, brighter, brightest? Why a display backlight system is more than meets the eye

To begin with, the human eye doesn’t perceive light in a linear way. So, if you’re looking to achieve a super-bright result, your display will need a huge amount of energy – more than double, in fact. For energy critical devices, this often means compromising brightness for battery life and the decision is taken to run with a low brightness display.
COM-Express-C10M-ALN

Avnet’s Latest MSC C10M-ALN Module Features the Intel Atom* Processor x7000E Series

January X, 2024 – The new MSC C10M-ALN module from Avnet (Nasdaq: AVT), is a COM Express Type 10 module that features the Intel Atom* processor x7000E Series of products including the Intel Core* i3 processor and Intel Processor N Series (codenamed Alderlake N). The CPU architecture is based on the same efficient cores and Intel UHD graphics driven by Xe architecture as the 12th Gen Intel Core* processors, thus enabling application migration across Intel CPU performance and power ranges.