SM2S-AL Machine#

This machine is to be used for 64 bits, Apollo Lake-based SoMs.

Images using this machine can be easily emulated with QEMU, but such emulation may lack specific peripherals. As such, do not use the emulator to test hardware-dependent features, but rather purely software features.

This machine supports the VPX gstreamer plugin, which allows for hardware accelerated VP8 and VP9 decoding. They are also built with support for the SD8887 WLAN/Bluetooth card.