- ...
- base images
- SDK
- ...
Getting the IP address of the board#
Once booted, the board will automatically setup the network interfaces using
DHCP. You can get the board ip address by logging as root
on a debug
console and running the ip address
command. Here is an example where the
target ip is 192.168.122.81
ip address
1: lo: <LOOPBACK,UP,LOWER_UP> mtu 65536 qdisc noqueue qlen 1000
link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00
inet 127.0.0.1/8 scope host lo
valid_lft forever preferred_lft forever
2: ETH0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc fq_codel qlen 1000
link/ether 52:54:00:ae:0f:5f brd ff:ff:ff:ff:ff:ff
inet 192.168.122.81/24 brd 192.168.122.255 scope global dynamic enp0s3
valid_lft 3544sec preferred_lft 3544sec
In case you cannot connect the device and your computer to a network providing DHCP, see I cannot connect the device to my network
Tip
If you don’t have a serial terminal available, you can as well use our SimpleSwitch™-launcher