• ...
  • base images
  • SDK
  • ...

I don’t have a physical display available#

If you do not have a physical display at hand, you can still work with graphical applications using VNC on Linux or Remote Desktop on Windows, to see you graphical application.

Steps needed:

Now you should be able to connect to your board, using either VNC or Remote Desktop and see your application running without a physical screen attached

Screen dimensions

The size of the screen is determined by the configured display overlay, so different overlays might result in different resolutions being presented