- ...
- SDK
- Yocto
- ...
- ...
- tools
- debug
- package
- deploy
- debug
Deploy a SimpleSwitch™ package#
When using the SDK, it is recommended to deploy using the
simpleswitch-deploy-package simpleswitch-example <board_ip> -u --start
cd build
scp simpleswitch-example.ext4 root@<board_ip>:/apps
scp simpleswitch-example.simpleswitchpackage root@<board_ip>:/apps
ssh root@<board_ip> simpleswitch-install /apps/simpleswitch-example.simpleswitchpackage
ssh root@<board_ip> reboot
With QEMU#
When using QEMU, simply copy the SimpleSwitch™ package files in the apps folder instead
cd ${BUILD_DIR}/tmp/deploy/images/qemux86-64
cp simpleswitch-example.ext4 <vm_name>_apps
cp simpleswitch-example.simpleswitchpackage <vm_name>_apps/simpleswitch-manifest.yaml
# Note ``<vm_name>_apps`` might be in a subdirectory if the tar.bz2 bundle was extracted in a subdirectory
sudo setfacl -m u:libvirt-qemu:rwx <vm_name>_apps/simpleswitch-example.ext4
virsh -c qemu:///system reboot <vm_name>
Note
One can check how to bundle and use a QEMU VM from our libvirt VM bundle tool section.
Detailed usage of simpleswitch-deploy-package#
simpleswitch-deploy-package --help
Usage: simpleswitch-deploy-package [options] package target_address
Options:
-u|--allow-update # Allow to reuse files from the previous build.
-w|--work-dir # Set the output directory.
-s|--start # Start the application after deployment.