How can I test my SDK extension?#
How can I test my SDK extension?
I have a new or changed SDK extension, how can I test it?
Run against the base SDK
You will need to run your test with the base SDK (simplecore-simpleswitch-sdk).
First create a new test case at lib/oeqa/sdk/cases/mytest.py with
the following content
from oeqa.extensions.helper import SimpleCoreTestExtensions
from oeqa.sdk.case import OESDKTestCase
class SimpleSwitch_SDKTests_MyTest(OESDKTestCase):
def setUp(self):
"""Check preconditions."""
self._version = os.environ.get('OECORE_SDK_VERSION', 'latest')
if self._version == '0.1.0':
self._version = 'latest'
def test_simpleswitch_mytest_package(self):
SimpleCoreTestExtensions.sdk.install_extension(self, 'mysdk', self._version)
mysdk is the value of SIMPLESWITCH_SDK_EXTENSION_NAME you set.
Next build your base SDK and your extension
$ scotty build simplecore-simpleswitch-sdk simpleswitch-sdk-ext-mytest -c populate_sdk
Now you can then run tests against the the base SDK + the requested extension, using the guide at How can I test my changes to the SDK test cases?