libvirt VM bundle tool#
scotty_vm_bundle.sh script will generate a tar.bz2 archive containing the kernel, the
rootfs and a script to define a QEMU VM in libvirt.
Installation#
Installing scotty_vm_bundle.sh can be easily done with pip as part of the official
Scotty tool bundle.
$ pip install --user avnet-scotty
upgrading an existing installation can be done with:
$ pip install --user --upgrade avnet-scotty
Dependencies#
In order for the script to work, it requires libvirt to be installed both on the
machine that is used to create the bundle and on the target machine.
To install dependencies you can use the following commands :
$ sudo apt install qemu-system libvirt-daemon-system virtinst virt-viewer
$ sudo yum install qemu-kvm libvirt virt-install virt-viewer
Setup#
To fully enable QEMU, please perform the following operations.
Add user to libvirt group:
$ sudo adduser $USER libvirt
Start default network if not already started:
$ sudo virsh net-list --all
$ sudo virsh net-start default # only if network 'default' is inactive
Grant user libvirt-qemu the right access permissions:
$ sudo setfacl -m u:libvirt-qemu:r-x ${BUILD_DIR}/tmp/deploy/images/qemux86-64
After this, a logout out of your current user session is required.
How to use#
The syntax of calling scotty_vm_bundle.sh is the following:
$ cd ${BUILD_DIR}/tmp/deploy/images/qemux86-64
$ scotty_vm_bundle.sh <vm_name> <kernel> rootfs.ext4
where <vm_name> is the name of the vm that is going to be created, <kernel> is the
kernel image and rootfs.ext4 is the rootfs image produced by Yocto.
For example:
$ cd /home/$USER/build/build/tmp/deploy/images/qemux86-64
$ scotty_vm_bundle.sh my_vm \
bzImage-qemux86-64.bin \
simplecore-weston-demo-image-qemux86-64.ext4
Calling scotty_vm_bundle.sh will produce <vm_name>_bundle.tar.bz2 archive that contains
the kernel, the rootfs and the scotty_vm_bundle.sh script.
Then, create a new folder and extract the <vm_name>_bundle.tar.bz2 archive to that
folder:
$ mkdir my_vm
$ tar -xj my_vm_bundle.tar.bz2 -C ./my_vm
Go to the new folder and call scotty_vm_bundle.sh:
$ cd my_vm
$ ./scotty_vm_bundle.sh [vm_name]
The script will create a VM in libvirt.
scotty_vm_bundle.sh accepts two optional arguments:
vm_nameto override the default VM name.
The VM can then be started:
$ virsh -c qemu:///system start my_vm
$ virsh -c qemu:///system console my_vm
One can get a graphic interface (only if the VM has been created from a graphic image bundle):
$ virt-viewer -c qemu:///system my_vm
Other useful commands:
$ virsh -c qemu:///system shutdown my_vm
$ virsh -c qemu:///system reboot my_vm
To remove the bundle:
$ virsh undefine my_vm