- ...
- base images
- SDK
- ...
- ...
- premade packages
SimpleSwitch™-terminal#
SimpleSwitch™-terminal (simplevte.py) is a helpful application that offers a way to open a terminal session
in base Yocto linux (
-)in any running SimpleSwitch™ containers, by using the
simpleswitch-interactivecommand
If a container starts it will be added as a “tab”, conversely if it stops then its “tab” will be removed.
SimpleSwitch™-terminal icon is in the top-left of the screen - near the small Tria logo, and next to the screenshot icon. SimpleSwitch™-terminal has touchscreen support, via the on-screen virtual keyboard.
The terminal configuration can be modified by placing /usr/share/simplevte/simplevte.config in $HOME - where it can be customised.
The [DEFAULT] items can be modified, but should not be deleted.
Tip
SimpleSwitch™-terminal is only available in graphical base images