- ...
- Yocto
- production
- project creation
- SDK extension
- SimpleSwitch
SDK extension#
To define a SDK extension you will need to create the following:
First a new SDK flavor and then create a new file simpleswitch-sdk-ext-<flavor>.bb in your layer, with the
following content
SUMMARY ?= "Simpleswitch SDK <flavor> extension"
inherit simpleswitch-sdk-extension-image
SIMPLESWITCH_SDK_EXTENSION_NAME = "<flavor>"
and run the build with
scotty build simpleswitch-sdk-ext-<flavor>
after that the installer to your extension will be available at build/build/tmp/deploy/sdk/ and can be used to install From a local installer.
Automatically publish to GHCR#
To publish the extension to Tria’s GHCR add a new file simpleswitch-sdk-ext-<flavor>-container.bb in your layer, with the
following content
SUMMARY ?= "Simpleswitch SDK <flavor> extension container"
inherit simpleswitch-sdk-extension-container
SDK_EXTENSION_NAME = "<flavor>"