• ...
  • SDK
  • Yocto
  • ...
  • ...
  • tools
  • debug
  • package
  • deploy
  • debug

Debug features#

SimpleSwitch™ debug features of the package can be enabled using the --debug parameter. So far the only debug feature enabled in this mode is Live update in QEMU, exporting package filesystem over NFS during runtime.

Note

The debug features do not enable software debugging tools such as GDB. Using these tools can be controlled through the startup command.