Build the project using an external tool#
You can also build with any external tool and create a package by copying the content of a directory. All you need is this directory to reproduce the structure desired in the package.
Assuming that your external tool uses deploy_dir to store its output, we would
require a directory structure like
find deploy_dir -printf "%y %p\n"
d deploy_dir
d deploy_dir/usr
d deploy_dir/opt/c_test_prog
f deploy_dir/opt/c_test_prog/c_test_prog
which mimics the structure of a linux root file system tree.
You can then use the --copy-dir option of the
simpleswitch-generate-package the
Generate a SimpleSwitch™ package
simpleswitch-generate-package --name simpleswitch-example --copy-dir deploy_dir \
--template C --startup-command /opt/c_test_prog/c_test_prog
Or if you want to be able to debug your application:
simpleswitch-generate-package --name simpleswitch-example --copy-dir deploy_dir \
--template C --startup-command "while true; do gdbserver :2159 /opt/c_test_prog/c_test_prog ; done"