- ...
- base images
- SDK
- ...
- setup hardware
- configure
- ...
- download
- flash
- configure hardware
Configure base board and external hardware via SimpleSwitch™-launcher#
You will need…
a computer
our Launcher
a network connection of the board
a Github personal access token (see Github container registry (GHCR))
If your device already shows a desktop on your display, please proceed with SimpleSwitch™-launcher on the device. If not please refer to Windows and Linux app.
Select the matching base board
To select the matching base board, click on Configuration and then Base Boards in the left side menu
Select the matching display
To select the matching display, click on Configuration and then Displays in the left side menu