- ...
- SDK
- Yocto
- ...
- ...
- tools
- debug
- package
- deploy
- debug
SimpleSwitch™ manifest#
The SimpleSwitch™ manifest acts as the entry point of the SimpleSwitch™ configuration. This is a YAML document describing the different packages. It will be automatically generated by Yocto or the SDK on application package creation.
Here is an example manifest
simpleswitch-hello-world:
description: A minimal container image.
license: MIT
dependencies: []
system_requirements: []
package_prefix: simpleswitch-hello-world
debug: '0'
maxsize: -1
autostart: true
simpleswitch-python-hello-world:
description: A minimal python container image.
license: MIT
dependencies: [simpleswitch-hello-world]
system_requirements: [wayland]
package_prefix: simpleswitch-python-hello-world
debug: '1'
maxsize: 10000000
autostart: true
bindmounts: /apps/foo:/apps/bar
Options explained#
See also