• ...
  • SDK
  • Yocto
  • ...
  • ...
  • tools
  • debug
  • package
  • deploy
  • debug

Manage SimpleSwitch™ packages#

Some scripts are here to ease the manipulation of SimpleSwitch™ applications:

  • simpleswitch-status to get the status of SimpleSwitch™ applications.

  • simpleswitch-start-package to start a SimpleSwitch™ application and its dependencies.

  • simpleswitch-stop-package to stop a SimpleSwitch™ application.

  • simpleswitch-enable-package to enable the automatic start on boot of a SimpleSwitch™ application and start it and its dependencies.

  • simpleswitch-disable-package to disable the automatic start on boot of a SimpleSwitch™ application and stop it.

The last 4 scripts need exactly 2 parameters:

  • the SimpleSwitch™ application

  • the IP address of the target

The simpleswitch-status can be used with these 2 parameters to return the status of the given SimpleSwitch™ application. But it could also be used just passing the IP address of the target. In this case, the status of all installed SimpleSwitch™ application is displayed, example:

simpleswitch-status 192.168.0.32
Warning: Permanently added '192.168.0.32' (RSA) to the list of known hosts.
INFO: SIMPLESWITCH APPS               AUTOSTART       ACTIVE STATE    SUB STATE       RESULT          MAIN PID
INFO: simpleswitch-A                  False           inactive        dead            success         834
INFO: simpleswitch-B                  True            active          running         success         994
INFO: simpleswitch-C                  True            failed          failed          exit-code       1572

Removing a deployed package can be done using the following command

simpleswitch-remove-package simpleswitch-example 192.168.0.32