runqemu#
usage: scotty runqemu [-h] [-t] [--nographic] [--extra-args EXTRA_ARGS]
target [target ...]
Run image in QEMU
positional arguments:
target Target to run
options:
-h, --help show this help message and exit
-t, --testimage Run testimage (default: False)
--nographic Disable graphics (default: False)
--extra-args EXTRA_ARGS
Optional extra arguments (default: [])
Note
It is recommended to run this command via the scotty-runqemu script from your host,
as this will setup all the needed arguments for a seamless interaction with the Docker
container