- ...
- Yocto
- production
- project creation
- SDK extension
- SimpleSwitch
Create a custom SDK#
A new SDK can be generated using the bitbake command
## On your computer run
scotty build simplecore-simpleswitch-sdk -c populate_sdk
## On your computer run
bitbake simplecore-simpleswitch-sdk -c populate_sdk
Registration
If you want to test SimpleCore™, SimpleSwitch™ or any of our packages from our SimpleCore™ incubator program, please register here and we will grant you access.
Adding packages to the target SDK#
In case you need additional packages in for the target device in your SDK, create a
`simplecore-simpleswitch-sdk.bbappend with the following content
TOOLCHAIN_TARGET_TASK:append = " package-one package-two"
This will make the content of package-one and package-two available for instance to the cross-compiler in the SDK.
Adding packages to the host SDK#
In case you need additional packages in for the host in your SDK, create a
simplecore-simpleswitch-sdk.bbappend with the following content
TOOLCHAIN_HOST_TASK:append = " package-one package-two"
This will make the content of package-one and package-two available directly to the user when the SDK got activated.