- ...
- Yocto
- production
- project creation
- SDK extension
- SimpleSwitch
Introduction to scotty#
You will need…
a computer with internet access
a git server of your choice
our
scottytool
For SimpleCore™ and SimpleSwitch™ we encourage to use our Scotty tool, that will help you to setup a fully configured Yocto workspace on your development machine.
Install scotty
First step is to install scotty.
See Getting started for more details.
scotty setup
now you can run
scotty setup
See Choosing the project options for more.
Choose SimpleSwitch feature
Make sure you are selecting SimpleSwitch as a feature.
If you forgot that, you can rerun the configuration at any time with
scotty --reconfigure setup
Build a base image
To create most of the build artifacts, we recommend to build
scotty build simplecore-simpleswitch-os-weston-image
scotty build simplecore-simpleswitch-os-image
That can take a while
Depending on
your internet connection speed
your CPU count
and your RAM
this can take up to a few hours of time.
In case the build is interrupted at any point, just retry the command
Now you can proceed to Build and integrate with Yocto to setup your own project.