Documentation build configuration#
In each repository a file called .scotty-docbuilds can be placed.
It contains a dictionary of the builds that should be done, when this
repository is part of the manifest.
Each key of the dictionary looks like this
"<build name, as shown in the github UI>"": {
"<key>": "<value>",
...
},
Each node is a key-value map just altering the values that are specific to this particular build (the rest will remain on sane default values). Please make sure that only strings are used.