- ...
- Yocto
- production
- project creation
- SDK extension
- SimpleSwitch
SDK templates packages#
Template packages are used as a base to generate SimpleSwitch™ packages using the Generate a SimpleSwitch™ package.
A few of them already exist, but you can modify them or create your own.
Creating a new package template is as easy as creating any Yocto image, with two extra constraints:
There name must be in the format
simpleswitch-NAME-template.bb, where NAME will be used with the--templateparameter of the package creation script.They must inherit from
simpleswitch-package-templateclass.
Here is the code of simpleswitch-flutter-template.bb the recipe for the flutter template installed in the SDK.
# SPDX-FileCopyrightText: (C) 2022 Avnet Embedded GmbH
# SPDX-License-Identifier: LicenseRef-Avnet-OSS-1.0
LICENSE = "Avnet-OSS-1.0"
inherit simpleswitch-package-template
IMAGE_INSTALL += "flutter-wayland-client flutter-engine flutter-runner"
SIMPLESWITCH_INSTALL_DEJAVU_FONTS_BASE = "1"
SIMPLESWITCH_INSTALL_DISPLAY_DRIVERS = "1"