Managing wired connection with systemd-networkd#
Systemd package supposed to contain all the necessary parts to operate wired network.
Wired network with static IP#
Create a file /etc/systemd/network/20-wired.network with following content:
[Match]
Name=ETH0
[Network]
Address=10.1.1.2/24
Gateway=10.1.1.1
DNS=10.1.1.1
Change Name key for desired adapter, change Address, Gateway and
DNS key for desired static IP address, gateway and DNS server.
Wired network using DHCP#
Create a file /etc/systemd/network/20-wired.network with following content:
[Match]
Name=ETH0
[Network]
DHCP=yes
Change Name key for desired adapter.
Configuration files#
The global configuration file in /etc/systemd/networkd.conf may be used to
override some defaults. Configuration files are located in
/usr/lib/systemd/network/, the volatile runtime network directory
/run/systemd/network/ and the local administration network directory
/etc/systemd/network/. Files in /etc/systemd/network/ have the highest
priority.
Rules are:
If all keys in the
[Match]section are matched, the profile is activatedan empty
[Match]section equivalent to*wildcard, profile is active alwaysall configuration files are collectively sorted and processed in lexical order, regardless of the directory in which they live
files with identical name replace each other
Meaning of particular keys can be obtained from official systemd-networkd documentation.