How can I test my changes to the SDK test cases?#
How can I test my changes to the SDK test cases?
I’ve written some changes to some SDK test cases and I want to test them locally, how is that possible?
Run SDK tests
When using a real piece of hardware you can run the following from
a scotty shell environment
$ bitbake <image-name> -c do_testcustomsdk
runtime cases only
This method applies only the test cases defined under lib/oeqa/sdk/cases
Grab a coffee
Depending on how many test cases are configured for the chosen image, running the test suite can take a while. So it might be the perfect time to grab a coffee.