Build configuration#
In each repository a file called .scotty-builds can be placed.
It contains a dictionary of the builds that should be done, when this
repository is part of the manifest.
Each key of the dictionary looks like this
"<build name, as shown in the github UI>"": {
"<key>": "<value>",
...
},
Each node is a key-value map just altering the values that are specific
to this particular build (the rest will remain on sane default values).
Please make sure that only strings are used.
Every key that starts with _ will be stripped from the output.