- ...
- base images
- SDK
- ...
- ...
- tools
- premade packages
simpleswitch-helper install/uninstall#
simpleswitch-helper install --help
usage: simpleswitch-helper install [-h] fragment
positional arguments:
fragment Path to the manifest fragment
options:
-h, --help show this help message and exit
can be used to install a SimpleSwitch™ package stored on the device.
The path to the simpleswitch.package file of the new package needs to be passed.
Note
The filesystem image of the package (.ext4 or .squashfs) needs to be in the same folder as
the simpleswitch.package file.
To uninstall an installed package run
simpleswitch-helper uninstall --help
usage: simpleswitch-helper uninstall [-h] app
positional arguments:
app The application to uninstall
options:
-h, --help show this help message and exit