- ...
- SDK
- Yocto
- ...
- ...
- tools
- debug
- package
- deploy
- debug
Generate a SimpleSwitch™ package#
The simpleswitch-generate-package script helps to create SimpleSwitch™
packages from existing templates, without requiring to use Yocto. It will merge
the template files and your own file to generate a SimpleSwitch™ package and its
manifest fragment.
SimpleSwitch™ Package Creation Example#
Copying your own files over the SimpleSwitch™ template can be done using the following command
simpleswitch-generate-package --name simpleswitch-example --copy-dir deploy_dir \
--template c --startup-command /usr/bin/c_test_prog
- This will generate two files:
simpleswitch-example.ext4: A filesystem containing the merge of the template and your files. It needs to be deployed in the/appsfolder of the target.simpleswitch-example.simpleswitchpackage: A fragment of SimpleSwitch™ manifest. It needs to be concatenated to the/apps/simpleswitch-manifest.yamlfile on the target.
Directory deploy_dir must contain all files to copy in the package, in a
structure reflecting its hierarchy in the package
find deploy_dir -printf "%y %p\n"
d deploy_dir
d deploy_dir/usr
d deploy_dir/usr/bin
f deploy_dir/usr/bin/c_test_prog
template can be changed according to the desired template, run
simpleswitch-generate-package --help to list all supported templates.
Finally, the startup command is specified using the --startup-command
parameter.
Advanced usage#
Detailed usage of simpleswitch-generate-package#
usage: simpleswitch-generate-package [-h] [--api-doc API_DOC] [--description DESCRIPTION] [--license LICENSE] [--reboot-required {0,1}]
[--size-factor SIZE_FACTOR] [--system-requirements [SYSTEM_REQ ...]] [-a [BIND_PATH ...]]
[-C [COPY_DIRS ...]] [-d] [-D [DEPENDS_ON ...]] [-I INSTALL_COMMAND] [-m [MAKEFILE_DIRS ...]] -n NAME
[-N] [-p STORAGE_SIZE] [-r SYSROOT_DIR] [-S SIZE] -s STARTUP_COMMAND -t TEMPLATE [-u]
[-U UNINSTALL_COMMAND] [-w WORK_DIR]
options:
-h, --help show this help message and exit
--api-doc API_DOC Path to API document (default: None)
--description DESCRIPTION
Description of the package (default: )
--license LICENSE License of the package in SPDX notation (default: Avnet-OSS-1.0)
--reboot-required {0,1}
Package requires a reboot on install/uninstall (default: 0)
--size-factor SIZE_FACTOR
Overhead factor of filesystem (default: 1.2)
--system-requirements [SYSTEM_REQ ...]
Base image features required (default: [])
-a [BIND_PATH ...], --bind-path [BIND_PATH ...]
Bind mount (default: [])
-C [COPY_DIRS ...], --copy-dir [COPY_DIRS ...]
Directories to copy into the roots (default: [])
-d, --debug Enable debugging (default: False)
-D [DEPENDS_ON ...], --depends-on [DEPENDS_ON ...]
Packages required (default: [])
-I INSTALL_COMMAND, --install-command INSTALL_COMMAND
Command on installation (default: )
-m [MAKEFILE_DIRS ...], --makefile-dir [MAKEFILE_DIRS ...]
Directories with makefiles (default: [])
-n NAME, --name NAME Name of the package (default: None)
-N, --no-autostart Disable autostart (default: False)
-p STORAGE_SIZE, --storage-size STORAGE_SIZE
Size of persistent storage (default: -1)
-r SYSROOT_DIR, --sysroot SYSROOT_DIR
Sysroot (default: )
-S SIZE, --size SIZE Filesystem size (default: None)
-s STARTUP_COMMAND, --startup-command STARTUP_COMMAND
Startup command (default: )
-t TEMPLATE, --template TEMPLATE
Template to use (default: None)
-u, --allow-update Enable updating (default: False)
-U UNINSTALL_COMMAND, --uninstall-command UNINSTALL_COMMAND
Command on uninstallation (default: )
-w WORK_DIR, --work-dir WORK_DIR
Working directory (default: current working directory)
Tip
Tips for package generation
description can be a string or a file.
If it’s a file, the content will be used
All settings of bind-path, depends-on and system-requirements will be merged with the settings
provided by the SDK template for the chosen template style.
reboot-required setting passed, only become effective if the the setting
provided by the SDK template for the chosen template style, do not enforce that already.
api-doc should point to a markdown file within the workspace.
It can contain mermaid diagrams.