- ...
- base images
- SDK
- ...
- setup hardware
- configure
- ...
- download
- flash
- configure hardware
Flashing base images (QEMU)#
You will need…
a Linux computer
There is no need to flash the image for QEMU platform. We suggest using libvirt for this.
If you haven’t installed QEMU yet, please install the following packages
sudo apt install qemu-system libvirt-daemon-system virtinst virt-viewer
sudo yum install qemu-kvm libvirt virt-install virt-viewer
Setup#
To fully enable QEMU, please perform the following operations.
Add user to libvirt group:
sudo adduser $USER libvirt
Start default network if not already started:
sudo virsh net-list --all
sudo virsh net-start default # only if network 'default' is inactive
New user session required
After this, a logout out of your current user session is required.
How to create the VM#
Extract the QEMU libvirt bundle that can be found in our Base image downloads section.
Note
Another option is to use scotty to build simplecore-simpleswitch-os-image, a console
only image, or simplecore-simpleswitch-os-weston-image, a graphic image and create
your own bundle, as documented in our libvirt VM bundle tool section.
mkdir -p simpleswitch-vm
tar -xf bundle-02_qemux86-64-simpleswitch-os-simplecore-simpleswitch-os-image.bz2 -C simpleswitch-vm
cd simpleswitch && ./scotty_vm_create.sh
mkdir -p simpleswitch-vm
tar -xf bundle-02_qemux86-64-simpleswitch-os-simplecore-simpleswitch-os-weston-image.bz -C simpleswitch-vm
cd simpleswitch-vm && ./scotty_vm_create.sh
Note
One can pass option -s to scotty_vm_create.sh in order to create a shared folder <image_name>_apps/
between the QEMU VM and the host. This folder can be used to deploy SimpleSwitch™ containers on the QEMU VM.