- ...
- base images
- SDK
- ...
- ...
- tools
- premade packages
Automatic resizing of the SDCard#
By default the boot medium will be extended to cover the space of the physical medium. If you do not want that, you can deactivate the feature.
From the base image#
run on the device
echo "SIMPLESWITCH_SDCARD_NOGROW=1" >> /etc/hw-info
From Yocto#
By setting HW_INFO_VARS = "SIMPLESWITCH_SDCARD_NOGROW=1" in your local.conf the container partition will
be resized to the maximum available size of the boot medium.