• ...
  • base images
  • SDK
  • ...
  • ...
  • tools
  • premade packages

How to use I2C#

Attention

  • sm2s-al/sm2s-el may require some of I2C interfaces to be enabled in BIOS setup, see corresponding User Manual for SMARC module in question.

  • i2c-tools package should be installed on the target image if userspace access to I2C is required.

Bus information#

You can list available buses using following command

ls -l /dev/bus/i2c/by-id/
total 0
lrwxrwxrwx    1 root     root            14 Apr 28 17:42 I2C0 -> ../../../i2c-0
lrwxrwxrwx    1 root     root            14 Apr 28 17:42 SMBUS -> ../../../i2c-1
lrwxrwxrwx    1 root     root            15 Apr 28 17:42 UNKNOWN_10 -> ../../../i2c-10
lrwxrwxrwx    1 root     root            15 Apr 28 17:42 UNKNOWN_11 -> ../../../i2c-11
lrwxrwxrwx    1 root     root            15 Apr 28 17:42 UNKNOWN_12 -> ../../../i2c-12
lrwxrwxrwx    1 root     root            15 Apr 28 17:42 UNKNOWN_13 -> ../../../i2c-13
lrwxrwxrwx    1 root     root            14 Apr 28 17:42 UNKNOWN_2 -> ../../../i2c-2
lrwxrwxrwx    1 root     root            14 Apr 28 17:42 UNKNOWN_3 -> ../../../i2c-3
lrwxrwxrwx    1 root     root            14 Apr 28 17:42 UNKNOWN_4 -> ../../../i2c-4
lrwxrwxrwx    1 root     root            14 Apr 28 17:42 UNKNOWN_5 -> ../../../i2c-5
lrwxrwxrwx    1 root     root            14 Apr 28 17:42 UNKNOWN_6 -> ../../../i2c-6
lrwxrwxrwx    1 root     root            14 Apr 28 17:42 UNKNOWN_7 -> ../../../i2c-7
lrwxrwxrwx    1 root     root            14 Apr 28 17:42 UNKNOWN_8 -> ../../../i2c-8
lrwxrwxrwx    1 root     root            14 Apr 28 17:42 UNKNOWN_9 -> ../../../i2c-9
lrwxrwxrwx    1 root     root            14 Apr 28 17:42 USER -> ../../../i2c-0

USER bus is the general purpose bus exposed on a SMARC connector, other buses are special purpose, please see corresponding User Manual for information about other I2C buses available on your SMARC module.

Kernel drivers#

If kernel driver for particular I2C device exists and compiled in or compiled as a module, device should be claimed automatically. To check what devices are detected by kernel you can explore following sysfs path:

ls -l /sys/bus/i2c/devices/
total 0
lrwxrwxrwx    1 root     root             0 Apr 28 17:42 1-0050 -> ../../../devices/pci0000:00/0000:00:1f.4/i2c-1/1-0050
lrwxrwxrwx    1 root     root             0 Apr 28 18:32 1-0055 -> ../../../devices/pci0000:00/0000:00:1f.4/i2c-1/1-0055
lrwxrwxrwx    1 root     root             0 Apr 28 17:42 i2c-0 -> ../../../devices/pci0000:00/0000:00:19.0/i2c_designware.0/i2c-0
lrwxrwxrwx    1 root     root             0 Apr 28 17:42 i2c-1 -> ../../../devices/pci0000:00/0000:00:1f.4/i2c-1
lrwxrwxrwx    1 root     root             0 Apr 28 18:32 i2c-10 -> ../../../devices/pci0000:00/0000:00:02.0/i2c-10
lrwxrwxrwx    1 root     root             0 Apr 28 18:32 i2c-11 -> ../../../devices/pci0000:00/0000:00:02.0/drm/card0/card0-DP-1/i2c-11
lrwxrwxrwx    1 root     root             0 Apr 28 18:32 i2c-12 -> ../../../devices/pci0000:00/0000:00:02.0/drm/card0/card0-DP-2/i2c-12
lrwxrwxrwx    1 root     root             0 Apr 28 18:32 i2c-13 -> ../../../devices/pci0000:00/0000:00:18.0/i2c-13
lrwxrwxrwx    1 root     root             0 Apr 28 18:32 i2c-2 -> ../../../devices/pci0000:00/0000:00:02.0/i2c-2
lrwxrwxrwx    1 root     root             0 Apr 28 18:32 i2c-3 -> ../../../devices/pci0000:00/0000:00:02.0/i2c-3
lrwxrwxrwx    1 root     root             0 Apr 28 18:32 i2c-4 -> ../../../devices/pci0000:00/0000:00:02.0/i2c-4
lrwxrwxrwx    1 root     root             0 Apr 28 18:32 i2c-5 -> ../../../devices/pci0000:00/0000:00:02.0/i2c-5
lrwxrwxrwx    1 root     root             0 Apr 28 18:32 i2c-6 -> ../../../devices/pci0000:00/0000:00:02.0/i2c-6
lrwxrwxrwx    1 root     root             0 Apr 28 18:32 i2c-7 -> ../../../devices/pci0000:00/0000:00:02.0/i2c-7
lrwxrwxrwx    1 root     root             0 Apr 28 18:32 i2c-8 -> ../../../devices/pci0000:00/0000:00:02.0/i2c-8
lrwxrwxrwx    1 root     root             0 Apr 28 18:32 i2c-9 -> ../../../devices/pci0000:00/0000:00:02.0/i2c-9
lrwxrwxrwx    1 root     root             0 Apr 28 17:42 i2c-MEX0000:00 -> ../../../devices/pci0000:00/0000:00:1f.4/i2c-1/i2c-MEX0000:00
lrwxrwxrwx    1 root     root             0 Apr 28 17:42 i2c-MEX0008:00 -> ../../../devices/pci0000:00/0000:00:1f.4/i2c-1/i2c-MEX0008:00
lrwxrwxrwx    1 root     root             0 Apr 28 17:42 i2c-MSFT8000:00 -> ../../../devices/pci0000:00/0000:00:19.0/i2c_designware.0/i2c-0/i2c-MSFT8000:00

I2C Tools#

Most of I2C devices are handled by kernel drivers, however there is a userspace driver for I2C which can be accessed with tools provided by i2c-tools package.

To acquire information about available I2C interfaces

i2cdetect -l
i2c-0   i2c             Synopsys DesignWare I2C adapter         I2C adapter
i2c-0   *link*          I2C0                                    ID mapped
i2c-0   *link*          USER                                    ID mapped
i2c-1   smbus           SMBus I801 adapter at efa0              SMBus adapter
i2c-1   *link*          SMBUS                                   ID mapped
i2c-2   i2c             i915 gmbus dpa                          I2C adapter
i2c-2   *link*          UNKNOWN_2                               ID mapped
i2c-3   i2c             i915 gmbus dpb                          I2C adapter
i2c-3   *link*          UNKNOWN_3                               ID mapped
i2c-4   i2c             i915 gmbus dpc                          I2C adapter
i2c-4   *link*          UNKNOWN_4                               ID mapped
i2c-5   i2c             i915 gmbus tc1                          I2C adapter
i2c-5   *link*          UNKNOWN_5                               ID mapped
i2c-6   i2c             i915 gmbus tc2                          I2C adapter
i2c-6   *link*          UNKNOWN_6                               ID mapped
i2c-7   i2c             i915 gmbus tc3                          I2C adapter
i2c-7   *link*          UNKNOWN_7                               ID mapped
i2c-8   i2c             i915 gmbus tc4                          I2C adapter
i2c-8   *link*          UNKNOWN_8                               ID mapped
i2c-9   i2c             i915 gmbus tc5                          I2C adapter
i2c-9   *link*          UNKNOWN_9                               ID mapped
i2c-10  i2c             i915 gmbus tc6                          I2C adapter
i2c-10  *link*          UNKNOWN_10                              ID mapped
i2c-11  i2c             AUX B/DDI B/PHY B                       I2C adapter
i2c-11  *link*          UNKNOWN_11                              ID mapped
i2c-12  i2c             AUX C/DDI C (TC)/PHY C                  I2C adapter
i2c-12  *link*          UNKNOWN_12                              ID mapped
i2c-13  i2c             Synopsys DesignWare I2C adapter         I2C adapter
i2c-13  *link*          UNKNOWN_13                              ID mapped

To probe and detect which device addresses are available on the bus

i2cdetect -y -r SMBUS
 0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f
00:                         -- -- -- -- -- -- -- --
10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
30: 30 31 -- 33 34 35 -- 37 -- -- -- -- -- -- -- --
40: -- -- -- -- 44 -- -- -- -- -- -- -- -- -- -- --
50: 50 -- 52 -- UU UU -- -- -- -- -- -- -- -- -- --
60: UU -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
70: -- -- -- -- -- -- -- --

UU denotes a device claimed by kernel driver.

You can dump register content of a particular device using i2cdump tool. To dump registers from 0 to 0xf on the device with address 0x27.

i2cdump -r 0-0xf USER 0x27 b
WARNING! This program can confuse your I2C bus, cause data loss and worse!
I will probe file /dev/i2c-0, address 0x27, mode byte
Probe range limited to 0x00-0x0f.
Continue? [Y/n] y
     0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f    0123456789abcdef
00: 04 04 04 04 04 10 08 00 04 40 00 00 00 00 00 04    ???????.?@.....?

You can also read and write from/to device using i2cget and i2cset.

i2cget 0 0x27 4 b
WARNING! This program can confuse your I2C bus, cause data loss and worse!
I will read from device file /dev/i2c-0, chip address 0x27, data address
0x04, using read byte data.
Continue? [Y/n] y
0x04
i2cset 0 0x27 4 0x04 b
WARNING! This program can confuse your I2C bus, cause data loss and worse!
I will write to device file /dev/i2c-0, chip address 0x27,
data address 0x04, data 0x04, mode byte.
Continue? [Y/n] y