Flashing internal eMMC with uuu tool#
Download Site for uuu Universal Update Utility#
The NXP uuu tool (former: Manufacturing Tool, mfgtool) can be found at its
GitHub repo page
This location contains:
the source files including
uuuscripts to update the different media on the respective Device Under Test (DUT)some binaries for use with Windows and Linux
complete documentation in PDF format
Prerequisites#
You need to have the following available:
a PC running Windows or Linux; Administrator / sudo permissions are required.
Downloaded and installed
uuutoolkit from above locationuuu scripts
emmc_burn_loader.lstandemmc_burn_all.lstFor flashing U-Boot and SPL Loader: the file
imx-boot-<board name>-sd.bin-flash_<board version>from the yocto buildFor flashing a complete OS image: a ready-made Yocto SD card image, e.g.
<distro name>-<board name>.wicthe Device Under Test
Operation#
On the DUT target, set the
FORCE_RECOV#line to LOWSwitch the power supply on to the target.
Connect the DUT target to the Host PC via its USB Port 0
Available Operations#
The following operations on the DUT target have been successfully tested to date:
SPL / U-Boot update to eMMC#
This option only writes U-Boot and SPL loader to the eMMC of the DUT. Note that under Linux, the command requires root / sudo permissions:
uuu -b emmc_burn_loader.lst <loader-image>
Example:
sudo uuu -b emmc_burn_loader.lst imx-boot-sm2s-imx95-sd.bin-flash_a55_8GiB
Complete Programming of U-Boot + SPL and an OS image to eMMC#
This option writes U-Boot + SPL loader and a complete OS image to the eMMC of the DUT. Note that under Linux, the command requires root / sudo permissions:
uuu -b emmc_burn_all.lst <loader-image> <system-image>
Example:
sudo uuu -b emmc_burn_all.lst imx-boot-sm2s-imx95-sd.bin-flash_a55_8GiB simplecore-simpleswitch-os-weston-image-sm2s-imx95.wic
Flashing internal eMMC bootloader manually#
You may sometimes not be able to flash using USB serial download with uuu,
particularly when the target main board does not expose the FORCE_RECOV#
line.
In this case please build an image, e.g. core-image-minimal, flash to
the SDCard and boot the image.
login into the shell
run /boot/emmc_boot0_install.sh to install to boot partition 0 (default)
run /boot/emmc_boot1_install.sh to install to boot partition 1